How to install S32DS 3.4 into a docker image (command line)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install S32DS 3.4 into a docker image (command line)

1,906 Views
maohuynh
Contributor II

Hello

My company needs to do continuous integration of our (S32K344 based) product's firmware. In order to make an easily reproducible build environment I'm trying to install S32DS 3.4 into a docker (windows server core) container. Within this container environment I have no GUI; it's command line only.

I see in the installation guide that "Installing the product from the command line in the console or silent mode is not supported."

Is there any way to accomplish installing S32DS without a GUI? If not, can anyone please suggest a way to get S32DS installed into a Docker container, or some other alternative to using S32DS to perform the Import, Generate, Build cycle?

Thanks

Mao Huynh

Tags (3)
0 Kudos
Reply
1 Reply

1,879 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately there is no other way. S32DS can be installed only with GUI. 

0 Kudos
Reply