"An Internal error has occurred" when update example project on .mex file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"An Internal error has occurred" when update example project on .mex file

Jump to solution
2,553 Views
MVR
Contributor V

Hello everyone,

I'm trying to update an example about SPI, using S32K344 and S32DS 3.4. The SDK version is 2.0.1.

This is the error that I'm facing:

MVR_0-1730211965441.png

In the past I was not facing this error, but it started suddenly... What should I do?

Thank you,

MVR

0 Kudos
Reply
1 Solution
2,526 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @MVR 

This error does not occur if you first removee SpiExternalDevice (SpiDriver tab) associated with SpiPhyUnit (SpiGeneral tab). 

Additionally, we recommend using the latest versions of RTD drivers in addition to the latest versions of the tools.

 

BR, VaneB

View solution in original post

0 Kudos
Reply
2 Replies
2,527 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @MVR 

This error does not occur if you first removee SpiExternalDevice (SpiDriver tab) associated with SpiPhyUnit (SpiGeneral tab). 

Additionally, we recommend using the latest versions of RTD drivers in addition to the latest versions of the tools.

 

BR, VaneB

0 Kudos
Reply
2,543 Views
MVR
Contributor V

I tried to reinstall the S32DS 3.4 and also the RTD S32K3XX 2.0.1 and still I'm facing the issue:

MVR_1-1730227660199.png

 

Basically I'm trying to remove the SpiPhyUnit_0 from the "Lpspi_Ip_HalfDuplexTransfer_S32K344" example...

0 Kudos
Reply