How to connect a new project to Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to connect a new project to Processor Expert

5,253件の閲覧回数
chljh
Contributor I

hello,

I install newest S32DS_ARM_Win32_v2018.R1_b180326, and create a new S32DS Application Project .

But the views of Processor Expert is empty!  And I cannot generate Processor Expert code!

please, Why?

1.png

2.png

thanks!

0 件の賞賛
返信
6 返答(返信)

4,473件の閲覧回数
ziomocci
Contributor IV

Hi all,

I get the same problem while creating a sample project for the S32K146 target, even if I select the SDK as suggested in the 1st response of @jiri_kral 

ziomocci_0-1604501631721.png

As you can see, SDK has been correctly selected, but when I click on Project-> generate Processor Expert Code

ziomocci_1-1604501734728.png

Any solution?

 

Thank you in advance,

 

Andrea Mocci

0 件の賞賛
返信

4,461件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Andrea, 

AMMCLIB doesn't contain processor expert - it is just library. If you like to use PE feature, you need to select for example S32_SDK_S32K1xx_RTM_3.0.0 SDK. 

 

Jiri

0 件の賞賛
返信

4,558件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Processor Expert is part of SDK - So, you need create new Project and add SDK. 

pastedImage_1.png

Jiri

0 件の賞賛
返信

4,558件の閲覧回数
chljh
Contributor I

Thank you for your reply.

我用的是KEA,这几天我试了各种方法,最后发现kds比s32ds更适合KEA。

I'm using KEA, and I tried several ways recently include of SDK1.3.  At last, I find that KDS is more suitable for KEA than s32ds.

我很奇怪为什么NXP在官网推荐用S32DS开发KEA而不是KDS。

I wonder why NXP recommends using S32DS to develop KEA instead of KDS on its official web.

0 件の賞賛
返信

4,558件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I see, unfortunately - SDK for KEA-128 in S32DS doesn't contain processor expert. If you need it - KDS is good choice. 

Jiri

0 件の賞賛
返信

4,558件の閲覧回数
davidrea
Contributor II

Where is this documented?!

First, Processor Expert isn't even mentioned in any of the manuals/guides accompanying S32DS. Short of finding this thread via Google, how are developers to know how to access the PEx functionality built into S32DS?

Second, where is the list of supported chips (SDKs?) for S32DS + PEx? The "Supported Devices" list on the S32DS product page just lists "KEA", implying that the whole family is supported. The lack of consistent device support across tools and SDKs is a major frustration with the Kinetis line as a whole.

Am I missing an obvious piece of documentation somewhere? Is there a big matrix somewhere that explains which tools and which SDKs support which processors? And is there a recommended Processor Expert-based workflow for KEAZ128 projects? (i.e. run standalone PEx and develop in S32DS?)

Thanks,
Dave