How to configure sampling point in CAN FD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure sampling point in CAN FD

4,158 Views
kimjunghyun
Contributor III

Hi.

I have to configure sampling point in CAN FD as below.

■ sampling point

   - Arbitration phase : 500K bit rate, 80% sampling point

   - Data phase : 2M bit rate, 75% sampling point

■ condition

   - CAN clock must be minimum 40MHz or more

■ MCU : S32K144(64pin)

But I could not configure sampling point as above.

I selected FIRC as CAN clock. 

 * the clock is selectable among 48, 52, 56, 60MHz

 * I could not use System OSC Clock because System OSC Range Select is up to 32MHz possible.

   CAN clock must be 40MHz or more. Refer to below picture.

11.jpg 

I configured these values automatically and manually on S32DS but I could not match these four values as above.

Is it possible to configure these values as above?

How should I configure?

some body help me please.

■ PE clock : 60MHz

60_A 500 80 D 2000 76.jpg

■ PE clock : 56MHz

56_A 500 81 D 2000 75.jpg

■ PE clock : 52MHz

52_A 500 76 D 2000 76.jpg

■ PE clock : 48MHz

48_A 500 81 D 2000 75_48m.jpg

Kim.

0 Kudos
Reply
0 Replies