Hi,
I got CSEc sample codes from below link.
http://www.nxp.com/docs/en/application-note-software/AN5401SW.zip
How do I compile these source code one by one in S32 Design studio ?
I am particular about compiling '4_secure_boot_add_BOOT_MAC_manual' in S32 Design studio environment.
Thanks
Mohan
已解决! 转到解答。
Hi Mohan,
Start S32DS for ARM, on the main menu bar click on File -> Import...
On the import window select General -> Existing project into Workspace
and select project which you are interested in
Now you can build it and upload into EVB for testing.
Jiri
Hi,
the example can be download here - https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true
If the link above doesn't work - just get the associated file from AN5401 pdf:
Jiri
Hi Mohan,
Start S32DS for ARM, on the main menu bar click on File -> Import...
On the import window select General -> Existing project into Workspace
and select project which you are interested in
Now you can build it and upload into EVB for testing.
Jiri