How to compile AN5401SW.zip in S32 Design studio for ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to compile AN5401SW.zip in S32 Design studio for ARM

Jump to solution
3,815 Views
mrajanna
Contributor V

Hi,

I got CSEc sample codes from below link.

http://www.nxp.com/docs/en/application-note-software/AN5401SW.zip

How do I compile these source code one by one in S32 Design studio ?

I am particular about compiling '4_secure_boot_add_BOOT_MAC_manual' in S32 Design studio environment.

 

Thanks

Mohan

Labels (2)
1 Solution
3,461 Views
jiri_kral
NXP Employee
NXP Employee

Hi Mohan, 

Start S32DS for ARM, on the main menu bar click on File -> Import...

s32ds_2017-08-07_12-35-52.png

On the import window select General -> Existing project into Workspace 

pastedImage_2.png

and select project which you are interested in

s32ds_2017-08-07_12-36-26.png

Now you can build it and upload into EVB for testing. 

Jiri 

View solution in original post

4 Replies
3,461 Views
mrajanna
Contributor V

Thank you Jiri. It worked.

0 Kudos
Reply
3,461 Views
pengchenbing
Contributor II

Could you share me the an5401sw.zip ?thanks!

0 Kudos
Reply
3,461 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the example can be download here - https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true 

If the link above doesn't work - just get the associated file from AN5401 pdf:

Search Results: AN5401 

Jiri

0 Kudos
Reply
3,462 Views
jiri_kral
NXP Employee
NXP Employee

Hi Mohan, 

Start S32DS for ARM, on the main menu bar click on File -> Import...

s32ds_2017-08-07_12-35-52.png

On the import window select General -> Existing project into Workspace 

pastedImage_2.png

and select project which you are interested in

s32ds_2017-08-07_12-36-26.png

Now you can build it and upload into EVB for testing. 

Jiri