Hi,
I am working with the S32K358 and using S32 Design Studio (S32DS) as my IDE. I would like to reserve specific memory regions for certain variables and ensure that these allocations are not affected by the compiler or linker during build time—especially when new variables or arrays are introduced later in the project.
I need to allocate a specific section of RAM exclusively for my own variables. These variables should be placed at fixed memory locations and must not be moved or overwritten by the compiler/linker during future software builds or updates.
I want to reserve areas in Flash or Data Flash for persistent data storage. For example:
Application_Valid_Flag
Bootloader_Valid_Flag
Arrays or structures containing configuration or runtime state data
These variables should be stored at fixed memory addresses and should remain unaffected by firmware reprogramming or section relocations—functioning similarly to EEPROM.
How can I configure the project settings in S32DS to reserve and assign specific memory addresses for variables (RAM, Flash, or Data Flash)?
How do I declare variables in code so they are placed into these custom-defined memory sections?
If S32DS or the compiler does not provide direct settings for this, how can I manually modify the linker script to define and reserve these specific memory areas?
Thanks and Regards,
Karmegan C
Hi @karmegancjk,
It depends on the compiler. For example, GCC does not support placing a variable directly at a specific address. Instead, GCC requires you to place variables in named sections, and then use the linker script to assign those sections to specific memory addresses.
Have a look at any RTD example, the linker file already defines multiple memory sections. You can create new sections by referencing these existing ones and extending them as needed.
For example, Placing a Variable in int_sram_no_cacheable:
#pragma GCC section bss ".mcal_bss_no_cacheable"
uint8_t variable;
#pragma GCC section bss
Here is an example that uses ITCM and DTCM and the linker file is modified because of that.
Regards,
Daniel
Hi Daniel,
If I place a variable in the int_pflash0 custom flash memory section or the int_dflash0 custom data flash memory section, how can I access that variable? Since writing to flash memory requires high-voltage operations, is it possible to write directly to variables placed in the flash or DFlash memory regions?
How can I verify whether the flash or DFlash memory region I created is correct?
Thanks and regards,
Karmegan C
Hi Karmegan C,
1.
It is not possible to write there.
The flash sector (0x2000 size) would need to be erased first.
You could use FEE driver on DFlash for non-volatile variables in flash.
2.
Check the .map file after compilation.
You should be able to locate the data names and their locations.
Regards,
Daniel