How do i build without error from project example vision sdk?? with sbc_s32v234

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do i build without error from project example vision sdk?? with sbc_s32v234

3,260 次查看
varun_kumar
Contributor II

When I tried to build some projects from the exiting project examples I'm getting following errors;

how will i be able to overcome this??kindly check in the attached pics

and

Could not determine GDB version using command: /opt/NXP/S32DS_Vision_v2.0/Cross_Tools/gcc-aarch64-linux-gnu-4_9/bin/aarch64-linux-gnu-gdb --version
/opt/NXP/S32DS_Vision_v2.0/Cross_Tools/gcc-aarch64-linux-gnu-4_9/bin/aarch64-linux-gnu-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory
 

Thanks in advance :smileyhappy:

0 项奖励
回复
1 回复

3,147 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you need to install some 32 bit libraries on your OS: 

pastedImage_1.png

More details you can find in pdf_getting_started.pdf manual located in 

[YOUR_S32DS_INSTALL_PATH]/S32DS/help/pdf . 

Hope it helps. 

Jiri 

0 项奖励
回复