How do I reference the default Workspace in the command line?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I reference the default Workspace in the command line?

ソリューションへジャンプ
5,984件の閲覧回数
roy_vanlierop
Contributor III

I'm automating my builds with the command line and I would like to use the same command across different machines. These machines have their Workspaces on different locations. They only use one Workspace. 

Where can I find (and reference) the default workspace? It it in a PATH variable, some .ini file or do I need to query some specific executable?

C:\NXP\S32DS.3.4\eclipse\eclipsec -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\local_projects\MyWonderfulWorkspaceS32DS -cleanBuild proj_name

0 件の賞賛
返信
1 解決策
5,974件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @roy_vanlierop ,

S32 Design Studio is built on top of Eclipse. As I am aware, Eclipse does not have a default workspace setting. S32DS does not add anything for this. Perhaps you could find some ideas in the Eclipse communities?

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,975件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @roy_vanlierop ,

S32 Design Studio is built on top of Eclipse. As I am aware, Eclipse does not have a default workspace setting. S32DS does not add anything for this. Perhaps you could find some ideas in the Eclipse communities?

Best Regards,

Mike

0 件の賞賛
返信
5,953件の閲覧回数
roy_vanlierop
Contributor III

Hello Mike, 

Thanks for the reply.

Except by making my own plugin there doesn't seem to be a straightforward way to get the workspace name. 

The workspace name is in the titlebar, I might be able to scrape it with some custom bat file. Seems like workaround. 

0 件の賞賛
返信
5,942件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @roy_vanlierop,

One thing you might consider, is having the workspace the same for all PCs. For example, the C:\Users\Public profile is on all Windows OS PCs, you could place the workspaces there and use the same name for the workspace in each case, then you would not need to implement a script to try to extract it. However, if you don't have influence over the humans that control each PC, perhaps the script is a better solution.

Mike

5,918件の閲覧回数
roy_vanlierop
Contributor III

Hi Mike,

This exactly my problem, the humans. 

I will cobble up some sort of script to extract the Workspace path. 

Thanks!

 

0 件の賞賛
返信