Greenhills plug in

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Greenhills plug in

Jump to solution
9,924 Views
leekate-b45752
NXP Employee
NXP Employee

Hello, 

Some errors occurred when I try to install GHS plug-in as below in S32DS 2018 R1 for ARM, could you check about it? 

And is there GHS plug-in install guidance material? 

pastedImage_2.png

Best regards,

Kate Lee

Tags (3)
0 Kudos
Reply
1 Solution
8,150 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, Rohan, 

 

As GHS is proprietary compiler provider, you would need to buy license for GHS. And you would need to install Greenhills "eclipse" plugin to use it on S32Design Studio. 

 

Also, please check this link for guide to use GHS plugin 

 

Please let us know if you face any further issue.

 

Thank you. Kind regards. 

 

- Mehul Patel 

 

View solution in original post

0 Kudos
Reply
5 Replies
8,218 Views
RohanD
Contributor I

Hello,

Can you please provide GHS Plugin that does support S32 design studio.

I tries connecting to the GHS team, they mentioned to get it from NXP.

I need it urgently.

0 Kudos
Reply
8,151 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, Rohan, 

 

As GHS is proprietary compiler provider, you would need to buy license for GHS. And you would need to install Greenhills "eclipse" plugin to use it on S32Design Studio. 

 

Also, please check this link for guide to use GHS plugin 

 

Please let us know if you face any further issue.

 

Thank you. Kind regards. 

 

- Mehul Patel 

 

0 Kudos
Reply
9,733 Views
stanish
NXP Employee
NXP Employee

Hi Kate,

Indeed you will  need a newer version of GHS plugin supported by neon v2.2.5+. See below:

pastedImage_1.png

Hope it helps.

Stan

0 Kudos
Reply
9,733 Views
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

If you already have GHS plugin compatible with Eclipse Neon - try to remove support for 68K/ColdFire - if you don't need it.. The error message looks that is related to this part only.  

Jiri

0 Kudos
Reply
9,733 Views
mikedoidge
NXP Employee
NXP Employee

Hi leekate-b45752‌,

The GHS Plugin does not support Eclipse Neon. S32 Design Studio for ARM migrated to Eclipse Neon in Release 2018.R1. If a user wishes to use the GHS Plugin on Eclipse Neon, then they must contact GreenHills support.

Best Regards,

Mike

0 Kudos
Reply