Greenhills plug in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
9,927件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hello, 

Some errors occurred when I try to install GHS plug-in as below in S32DS 2018 R1 for ARM, could you check about it? 

And is there GHS plug-in install guidance material? 

pastedImage_2.png

Best regards,

Kate Lee

タグ(3)
0 件の賞賛
返信
1 解決策
8,153件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, Rohan, 

 

As GHS is proprietary compiler provider, you would need to buy license for GHS. And you would need to install Greenhills "eclipse" plugin to use it on S32Design Studio. 

 

Also, please check this link for guide to use GHS plugin 

 

Please let us know if you face any further issue.

 

Thank you. Kind regards. 

 

- Mehul Patel 

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
8,221件の閲覧回数
RohanD
Contributor I

Hello,

Can you please provide GHS Plugin that does support S32 design studio.

I tries connecting to the GHS team, they mentioned to get it from NXP.

I need it urgently.

0 件の賞賛
返信
8,154件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, Rohan, 

 

As GHS is proprietary compiler provider, you would need to buy license for GHS. And you would need to install Greenhills "eclipse" plugin to use it on S32Design Studio. 

 

Also, please check this link for guide to use GHS plugin 

 

Please let us know if you face any further issue.

 

Thank you. Kind regards. 

 

- Mehul Patel 

 

0 件の賞賛
返信
9,736件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Kate,

Indeed you will  need a newer version of GHS plugin supported by neon v2.2.5+. See below:

pastedImage_1.png

Hope it helps.

Stan

0 件の賞賛
返信
9,736件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

If you already have GHS plugin compatible with Eclipse Neon - try to remove support for 68K/ColdFire - if you don't need it.. The error message looks that is related to this part only.  

Jiri

0 件の賞賛
返信
9,736件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi leekate-b45752‌,

The GHS Plugin does not support Eclipse Neon. S32 Design Studio for ARM migrated to Eclipse Neon in Release 2018.R1. If a user wishes to use the GHS Plugin on Eclipse Neon, then they must contact GreenHills support.

Best Regards,

Mike

0 件の賞賛
返信