Getting started with S32DS for Power 2.1 + MPC5777CEVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Getting started with S32DS for Power 2.1 + MPC5777CEVB

跳至解决方案
681 次查看
ricardofranca
Contributor III

Hello,

As suggested in the title, I have just installed S32DS to work with a MPC5777CEVB, which I have been successfully using with the Green Hills compiler suite and probe V4.

In my first glance at the documentation, I got a bit confused about the debugging environment: what are the possibilities for connecting the IDE to the board? I (think I) understood I would be able to do this using either an USB Multilink probe or a Lauterbach probe, and I would like to know if it is possible to use the Green Hills probe I already own or a simple USB connection (even if with reduced debugging capabilities).

Thanks,

Ricardo

 

标记 (1)
0 项奖励
回复
1 解答
659 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you need to use external JTAG debugger, simple USB cable connection is not possible here.

It does not seems this version of S32DS would have support for GHS debugger. 

Release notes only mentions 
- PEMicro debugger support (P&E Multilink/Cyclone/OpenSDA)
- Lauterbach Trace32 debugger support
- iSYSTEM debugger support
- PLS debugger support

and 

- Green Hills compiler support

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
1 回复
660 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you need to use external JTAG debugger, simple USB cable connection is not possible here.

It does not seems this version of S32DS would have support for GHS debugger. 

Release notes only mentions 
- PEMicro debugger support (P&E Multilink/Cyclone/OpenSDA)
- Lauterbach Trace32 debugger support
- iSYSTEM debugger support
- PLS debugger support

and 

- Green Hills compiler support

BR, Petr

0 项奖励
回复