GDB VLE Python support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GDB VLE Python support

2,817 Views
christopheple
Contributor II

Hi all,

Do you think, it could be possible to have Python support in powerpc-eabivle-gdb included in S32DS ?

Python offers many interesting scripting solution.

Is it the good place to request this kind of thing ?

Regards.

Labels (1)
0 Kudos
Reply
2 Replies

2,584 Views
stanish
NXP Employee
NXP Employee

Christophe,

Based on your feature request we have added the python GDB support into the latest release of S32DS for Power:

S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released! 

"<S32DS_Power_v2017.R1>\Cross_Tools\powerpc-eabivle-4_9\bin\powerpc-eabivle-gdb-py.exe"‍

Thank you,

S.

0 Kudos
Reply

2,584 Views
stanish
NXP Employee
NXP Employee

Hi Christophe,

Yes this is the right place to submit this request.

I logged this requirement/wish into our requirement database so this could be considered by the management.

Thank you!

Stan

0 Kudos
Reply