Freertos compilation error on Sd32 studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freertos compilation error on Sd32 studio

7,594 Views
prashantsathe
Contributor III

I am trying to build a project based on MAC57D54H (for M4 core). For this i have added basic freertos code. after successfully compiling 'c' code i am facing asm file compilation error. Could you please check this.

 

-------------------------------------------------------------------------------------------------------------------------------------------------------------

arm-none-eabi-gcc "@src/Demo/CORTEX_M4F_NXP_MAC57D5xx_MULTI/src_hello/common/m4_cache.args" -MMD -MP -MF"src/Demo/CORTEX_M4F_NXP_MAC57D5xx_MULTI/src_hello/common/m4_cache.d" -MT"src/Demo/CORTEX_M4F_NXP_MAC57D5xx_MULTI/src_hello/common/m4_cache.o" -c -o "src/Demo/CORTEX_M4F_NXP_MAC57D5xx_MULTI/src_hello/common/m4_cache.o" "../src/Demo/CORTEX_M4F_NXP_MAC57D5xx_MULTI/src_hello/common/m4_cache.c"

../src/Source/portable/MULTI/MAC57D5xx/portasm.s: Assembler messages:

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:72: Error: unknown pseudo-op: `.export'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:73: Error: unknown pseudo-op: `.export'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:74: Error: unknown pseudo-op: `.export'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:87: Error: junk at end of line, first unrecognized character is `-'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:93: Error: junk at end of line, first unrecognized character is `-'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:102: Error: junk at end of line, first unrecognized character is `-'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:114: Error: unshifted register required -- `tst lr,#0x10'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:116: Error: selected processor does not support Thumb mode `vstmdbeq r0!,{s16-s31}'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:119: Error: instruction not allowed in IT block -- `stmdb r0!,{r4-r11,r14}'

Finished building: ../src/Source/portable/MemMang/heap_5.c

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:124: Error: lo register required -- `stmdb sp!,{r3}'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:133: Error: lo register required -- `ldmia sp!,{r3}'

 

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:140: Error: lo register required -- `ldmia r0!,{r4-r11,r14}'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:144: Error: unshifted register required -- `tst r14,#0x10'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:146: Error: selected processor does not support Thumb mode `vldmiaeq r0!,{s16-s31}'

Finished building: ../src/Source/portable/MULTI/MAC57D5xx/port.c

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:148: Error: instruction not allowed in IT block -- `msr psp,r0'

 

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:152: Error: junk at end of line, first unrecognized character is `-'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:161: Error: lo register required -- `ldmia r0!,{r4-r11,r14}'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:168: Error: junk at end of line, first unrecognized character is `-'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:185: Error: junk at end of line, first unrecognized character is `-'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:190: Error: unexpected character `w' in type specifier

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:190: Error: bad instruction `ldr.w r0,CPACRConst'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:194: Error: unshifted register required -- `orr r1,r1,#(0xf<<20)'

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:98: Error: invalid offset, value too big (0xFFFFFFE8)

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:110: Error: invalid offset, value too big (0xFFFFFFCC)

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:125: Error: invalid offset, value too big (0xFFFFFFC8)

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:157: Error: invalid offset, value too big (0xFFFFFF94)

../src/Source/portable/MULTI/MAC57D5xx/portasm.s:173: Error: invalid offset, value too big (0xFFFFFF6C)

make: *** [src/Source/portable/MULTI/MAC57D5xx/portasm.o] Error 1

make: *** Waiting for unfinished jobs....

Finished building: ../src/Demo/CORTEX_M4F_NXP_MAC57D5xx_MULTI/src_hello/common/m4_cache.c

-------------------------------------------------------------------------------------------------------------------------------------------------------------

 

-Prashant

Labels (1)
0 Kudos
Reply
3 Replies

4,683 Views
prashantsathe
Contributor III

Portasm.s is attached.. current port is for IAR compiler, I am trying to port it on arm-none-eabi-gcc.

Would be helpful if you could point out the PATH to proceed, I am new to asm (only long back worked on ASM).

Error :-

=========================================================================

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s: Assembler messages:

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:94: Error: unshifted register required -- `tst lr,#0x10'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:96: Error: selected processor does not support Thumb mode `vstmdbeq r0!,{s16-s31}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:99: Error: instruction not allowed in IT block -- `stmdb r0!,{r4-r11,r14}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:104: Error: lo register required -- `stmdb sp!,{r3}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:112: Error: lo register required -- `ldmia sp!,{r3}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:119: Error: lo register required -- `ldmia r0!,{r4-r11,r14}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:123: Error: unshifted register required -- `tst r14,#0x10'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:125: Error: selected processor does not support Thumb mode `vldmiaeq r0!,{s16-s31}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:127: Error: instruction not allowed in IT block -- `msr psp,r0'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:147: Error: lo register required -- `ldmia r0!,{r4-r11,r14}'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:173: Error: unexpected character `w' in type specifier

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:173: Error: bad instruction `ldr.w r0,=0xE000ED88'

../src/FreeRtos/Source/portable/CORTEX_M4_MAC57D54H/portasm.s:177: Error: unshifted register required -- `orr r1,r1,#(0xf<<20)'

=========================================================================

Thanks,

Prashant

0 Kudos
Reply

4,683 Views
stanish
NXP Employee
NXP Employee

Hi Prashant,

I'd suggest you to add the assembler directive into portasm.s:

.syntax unified

https://sourceware.org/binutils/docs/as/ARM_002dInstruction_002dSet.html#ARM_002dInstruction_002dSet

enable floating point ABI:  hard

FPU Type: "fpv4-sp-d16"

Hope it helps.

Stan

0 Kudos
Reply

4,683 Views
stanish
NXP Employee
NXP Employee

Hi Prashant,

The GNU assembler (known as GAS) directives may differ from the ones located in your assembly file.

I'd suggest to use:

.global  instead of .export

.extern instead of .import

Could you attach your portasm.s if it does not help ?

Thanks.

Stan

0 Kudos
Reply