FreeMASTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeMASTER

Jump to solution
3,636 Views
renlei
Contributor I
0 Kudos
Reply
1 Solution
3,477 Views
stanish
NXP Employee
NXP Employee

Hi, 

I'd suggest to add path to appropriate driver .dll (e.g. ControlCAN.dll)  and test the connection. In  my case I also do not see any driver found but FreeMASTER works just fine with my ZLG compatible device.

Note: 

make sure there is no other application using ZLG device at the moment you are trying co use it in FreeMASTER.

pastedImage_1.png

hope it helps.

Stan.

View solution in original post

0 Kudos
Reply
1 Reply
3,478 Views
stanish
NXP Employee
NXP Employee

Hi, 

I'd suggest to add path to appropriate driver .dll (e.g. ControlCAN.dll)  and test the connection. In  my case I also do not see any driver found but FreeMASTER works just fine with my ZLG compatible device.

Note: 

make sure there is no other application using ZLG device at the moment you are trying co use it in FreeMASTER.

pastedImage_1.png

hope it helps.

Stan.

0 Kudos
Reply