FreeMASTER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,723件の閲覧回数
renlei
Fresh Out Contributor
0 件の賞賛
返信
1 解決策
3,564件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi, 

I'd suggest to add path to appropriate driver .dll (e.g. ControlCAN.dll)  and test the connection. In  my case I also do not see any driver found but FreeMASTER works just fine with my ZLG compatible device.

Note: 

make sure there is no other application using ZLG device at the moment you are trying co use it in FreeMASTER.

pastedImage_1.png

hope it helps.

Stan.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,564件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi, 

I'd suggest to add path to appropriate driver .dll (e.g. ControlCAN.dll)  and test the connection. In  my case I also do not see any driver found but FreeMASTER works just fine with my ZLG compatible device.

Note: 

make sure there is no other application using ZLG device at the moment you are trying co use it in FreeMASTER.

pastedImage_1.png

hope it helps.

Stan.

0 件の賞賛
返信