Flash tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash tool

1,871 次查看
Catherine
NXP Employee
NXP Employee

Hi expert,

 
 

image (1).jpg

 According to S32DS Flash tool guide, there is a target application which is located in the target SRAM. My device is S32Z and my question is

  1. When using S32DS Flash tool, what exact time dose target application is downloaded in SRAM? In other words, how to trigger host application to download target application to SRAM? My understanding is at the time clicking “Upload target and algorithm to hardware”
  2. where is the exact file of target application? Is it located in …\S32DS.3.5\S32DS\tools\S32FlashTool\flash? What is the file location of algorithm?
  3. According to the UG, “When done, the Boot ROM runs the Target Application on the selected CPU core of the device” When dose boot ROM boot the target core(I think smu-m33 core)? Dose boot ROM boot m33 core automatically after power on under serial boot mode?

 

Thank you very much for your support.

 

BR,

Catherine

 

 

标签 (1)
0 项奖励
回复
1 回复

1,846 次查看
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Catherine,

Please find my answers to your questions:

A1) You are correct, the time in which the application is loaded is when clicking the "Upload target and algorithm to hardware" to hardware button. However, the algorithm is not the first thing being loaded to the S32Z2 chip, the first biniry that gets load into the chip is in this case the S32Z2E2.bin file, which you can find in your installation directory, it should be similar to this: C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin.

If you check the command line approach you can see that when load the algorithm is loaded you need to select a binary corresponding to the chip, for example in my setup it would be:

S32FlashTool -t C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin -a C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\flash\S26HS512.bin,0,A -i uart -p COM27

The paths and COM number may change in your setup.

A2) I should have ansered the fisrt part of the second question in the first answer. For the algorithm path, you can find it in the following folder, for example for flash S26HS512, which is used in the S32Z2280-594EVB board: 

C:\NXP\S32DS.3.6.0\S32DS\tools\S32FlashTool\flash\S26HSom512.bin

A3) Your understanding is correct, the core responsible to run the serial application is the SMU/M33, you can see this in the reference manual [page 3219, S32Z2 Reference Manual, Rev. 3.1, 07/2024]:

alejandro_e_2-1741904351144.png

And for the whole program is loaded to the SRAM the core should be automatically started.

 

You can get a better perspective on how to interact with the S32FT operations by checking the command line options, you can get a "preconfigured" set of commands by setting up your S32FT GUI, for example:

alejandro_e_3-1741904685311.png

 

Then clicking on the "Launch command prompt" button:

alejandro_e_4-1741904734510.png

a windows command line instance will appear, and in it some commands already configured for your setup will be available:

# Retrieve existing COM ports
# S32FlashTool -i uart -p ?

# Retrieve connected, supported CAN adapters
# S32FlashTool -i can -p ?

# Retrieve Ethernet adapters
# S32FlashTool -i ethernet -p ?

# Load the target binary and read the MCUID
# S32FlashTool -t C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin -i uart -p COM27 -mcuid

# Load the target binary and the flash memory algorithm
# S32FlashTool -t C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin -a C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\flash\S26HS512.bin,0,A -i uart -p COM27

# Read 0x100 bytes from the address 0x0000_0000 of the flash memory
# S32FlashTool -t C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin -i uart -p COM27 -fread -addr 0x00000000 -size 0x100

# Upload (program) a file [FILE] to the flash memory starting with address 0x0000_0000
# S32FlashTool -t C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin -i uart -p COM27 -fprogram -addr 0x00000000 -f [FILE]

# Upload a binary [FILE] to SRAM at address [ADDRESS] and execute it
# S32FlashTool -t C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\targets\S32Z2E2.bin -i uart -p COM27 -addr [ADDRESS] -boot [FILE]

C:\NXP\S32DS.3.5\S32DS\tools\S32FlashTool\bin>

 

Please let me know if this information solved your questions.

0 项奖励
回复