Flash does not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash does not working

Jump to solution
2,892 Views
kbj
Contributor IV

Hi,

I use S32DS and S32K144.

When I test the flash write, I wrote the test data at adress 0x00.

After that, I can't flash program.

How to resolve it?

1.PNG

Labels (2)
1 Solution
2,738 Views
stanish
NXP Employee
NXP Employee

Hi,

Seems the flash configuration block was overwritten.

Please check this thread:

https://community.nxp.com/message/1062800#comment-1063606 

Are you able to connect and load your project into RAM (Debug RAM build config)?

Regards,

Stan

View solution in original post

2 Replies
2,739 Views
stanish
NXP Employee
NXP Employee

Hi,

Seems the flash configuration block was overwritten.

Please check this thread:

https://community.nxp.com/message/1062800#comment-1063606 

Are you able to connect and load your project into RAM (Debug RAM build config)?

Regards,

Stan

2,738 Views
kbj
Contributor IV

Dear Sliva,

Thanks for your help.

I solve it, Thanks to you. 

Best Regards,

Byungju.

0 Kudos
Reply