Flash does not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash does not working

ソリューションへジャンプ
2,933件の閲覧回数
kbj
Contributor IV

Hi,

I use S32DS and S32K144.

When I test the flash write, I wrote the test data at adress 0x00.

After that, I can't flash program.

How to resolve it?

1.PNG

ラベル(2)
1 解決策
2,779件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Seems the flash configuration block was overwritten.

Please check this thread:

https://community.nxp.com/message/1062800#comment-1063606 

Are you able to connect and load your project into RAM (Debug RAM build config)?

Regards,

Stan

元の投稿で解決策を見る

2 返答(返信)
2,780件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Seems the flash configuration block was overwritten.

Please check this thread:

https://community.nxp.com/message/1062800#comment-1063606 

Are you able to connect and load your project into RAM (Debug RAM build config)?

Regards,

Stan

2,779件の閲覧回数
kbj
Contributor IV

Dear Sliva,

Thanks for your help.

I solve it, Thanks to you. 

Best Regards,

Byungju.

0 件の賞賛
返信