Flash debugging option not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash debugging option not working.

6,307 Views
rajani_sureja33
Contributor III

Hi,

I am using S32 design studio ide for mpc5748g controller programing.

Here I am facing issue of flash debugging, I could not able to debug in flash.

While ram debug option working fine.

Attached screenshot of issue which i have facing. let me know what could be the reason?

Regards,

Rajani Sureja

Labels (2)
6 Replies

5,973 Views
jiri_kral
NXP Employee
NXP Employee

Hi Rajani, 

it looks that you are using old PE Micro plugin. Please update S3DS https://community.nxp.com/docs/DOC-342273  and try it again:

pastedImage_1.png

With latest version I have no issue on Linux host (Ubuntu 16.04 LTS)

Jiri

0 Kudos
Reply

5,973 Views
aniket_patel
Contributor I

Hi kral,

Thanks for quick replay.

I have Updated latest PE Micro plugin version(1.8.3.2018) in S32 Design studio but still s32 flash debugging option not working.

I think flash memory is locked. so flash debugging option not working.

can you please give me suggestion to resolve this problem.

0 Kudos
Reply

5,973 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can try PE Micro tool PROGPPCNEXUS to erase chip (unfortunately for windows only - but there is chance that this SW will work with Wine). You can find more details in this thread: 

https://community.nxp.com/message/1108728 

Hope it helps. 

Jiri 

5,973 Views
aniket_patel
Contributor I

Hi kral,

I will be purchasing one "PEmicro USB-ML-UNIVERSAL" programmer to erase Dev mpc5748g board and after is there board is working fine or not? Please check below programmer link which is I will purchase it.

Programmer Board Link:-> http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320168&productTab=5

0 Kudos
Reply

5,973 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

in my opinion debug probe doesn't solve your issue. MCU can be erased with existing OpenSDA interface. Just use steps described here - https://community.nxp.com/thread/494855

Jiri

0 Kudos
Reply

5,973 Views
aniket_patel
Contributor I

Thanks Jiri Kral, for resolved this problem.

0 Kudos
Reply