Failure in installing S32G support in S32DS 3.5.2 Linux version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failure in installing S32G support in S32DS 3.5.2 Linux version

1,677件の閲覧回数
AdrianGancev
NXP Employee
NXP Employee

I need to install S32DS with S32G support.

So I installed the S32DS.3.5_b220726_linux.x86_64.bin

Here the contents of the installation so far:

Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653
Package: S32 Design Studio Platform package; Version: 3.5.2; Build id: 202302262111
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202005201157
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853
Package: S32 Design Studio Platform Tools package; Version: 3.5.2; Build id: 202302262111
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521

When installing the S32G development package version 3.5.2, there is a failure as depicted below. How to solve this?

AdrianGancev_2-1685623021109.png

 

Cheers.

0 件の賞賛
返信
1 返信

1,669件の閲覧回数
AdrianGancev
NXP Employee
NXP Employee

I found that using the offline package of the same version of the S32G update site solved the problem. So you can investigate why the online installation failed.

0 件の賞賛
返信