Failure for debugging hello+pll

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failure for debugging hello+pll

3,655件の閲覧回数
hrfbit
Contributor II

what's wrong?

1.png2.png3.png

0 件の賞賛
返信
5 返答(返信)

3,364件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

I assume you are using S32DS Power and MPC5748G DevKit Board with OpenSDA interface.

I'd recommend you to install the latest S32DS Power + Update 1: 

S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released! 

S32 Design Studio for Power Architecture 2017.R1 - Update 1 available 

Then please check if the OpenSDA firmware is up-to-date (v1.10).  If not please update it:

HOWTO: Update OpenSDA Firmware on EVB 

Finally check if the board and MCU is powered up - 5V_OK and 3V3_OK LEDs are ON.

Hope it helps.

Stan

0 件の賞賛
返信

3,364件の閲覧回数
hrfbit
Contributor II

Google 翻译

I have completed all the above steps but it still does not work.
1.png
0 件の賞賛
返信

3,364件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

thanks for the update.

Could you create a new non-sdk project using project wizard build it and debug?

If it does not work there could be a hw issue - please check if the board is powered correctly (LEDs 5V_OK and 3V3_OK are on). If they are off please switch J1 jumper to 2-3 position.

pastedImage_4.png

Do you have an external debug probe to test e.g. P&E Multilink?

Stan

0 件の賞賛
返信

3,364件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Are you using S32DS for Power or ARM? Is your debugger OpenSDA or other? 

Jiri

0 件の賞賛
返信

3,364件の閲覧回数
hrfbit
Contributor II

OpenSDA

0 件の賞賛
返信