Failure for OpenSDA interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failure for OpenSDA interface

1,858件の閲覧回数
hrfbit
Contributor II

I am a new user for S32DS and trying to use S32DS Power and MPC5748G DevKit Board with OpenSDA interface to debug the "hello+pll". However, there was an error that the device could not be found as shown in the following pictrues.

2.png3.png

what's more, the version is shown as following:

1.png

In addition to this problem, I do not know where to learn the specific operation of debugging. Hope to get help form yours. Thank you!
0 件の賞賛
返信
2 返答(返信)

1,761件の閲覧回数
stanish
NXP Employee
NXP Employee
0 件の賞賛
返信

1,761件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you checked out the power? Are all three green LEDs at the end with Ethernet connector ON? If not and you are powering the board from USB - switch the Jumper (there is only one) to position close to ETH connector. 

Jiri 

0 件の賞賛
返信