Failure for OpenSDA interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure for OpenSDA interface

1,864 Views
hrfbit
Contributor II

I am a new user for S32DS and trying to use S32DS Power and MPC5748G DevKit Board with OpenSDA interface to debug the "hello+pll". However, there was an error that the device could not be found as shown in the following pictrues.

2.png3.png

what's more, the version is shown as following:

1.png

In addition to this problem, I do not know where to learn the specific operation of debugging. Hope to get help form yours. Thank you!
0 Kudos
Reply
2 Replies

1,767 Views
stanish
NXP Employee
NXP Employee
0 Kudos
Reply

1,767 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you checked out the power? Are all three green LEDs at the end with Ethernet connector ON? If not and you are powering the board from USB - switch the Jumper (there is only one) to position close to ETH connector. 

Jiri 

0 Kudos
Reply