Expected output for 'hello world' example on MPC5748G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Expected output for 'hello world' example on MPC5748G

1,831 次查看
sungjoonpark
Contributor I

Hello,

 

I am trying to work on the very first simple project on MPC5748G. I installed S32 Design Studio for Power Architecture, File - New - New S32DS Project, then selected hello world example. I expect that when I run the project, LEDs(DS4, 6 and 8) should blink or turn on. However, I do not see any changes on LEDs on the board. When I turn on the board, DS 4, 5, 6, 9 and 10 are turned on and they just stay on. and DS8 just stays off for the entire time. Could you please advise? or What am I expecting here from the project?

 

Thank you,

Sungjoon

标签 (1)
0 项奖励
回复
1 回复

1,510 次查看
martin_kovar
NXP Employee
NXP Employee

Hi Sungjoon,

these examples in S32 Design Studio are designed for the DEVKIT Evaluation board. DEVKIT Evaluation Board for MPC574xG|NXP

There are some differences in pin routing, so these example cannot be used for standard evaluation system.

From your description it seems you use standard evaluation system Evaluation System for MPC574xB/C/G Family|NXP.

So you have to edit GPIO settings for this board. Please look at the following example.

https://community.nxp.com/docs/DOC-330940 

If you have any other question, please feel free to write me back.

Regards,

Martin

0 项奖励
回复