Error with comand: gbd version for S32DS PA 2017 R1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error with comand: gbd version for S32DS PA 2017 R1

4,940件の閲覧回数
alex_yu1
Contributor III

Hello Guys,

      could you please help to check this issue for the S32 Design Studio for Power Architecture Version: 2017.R1 , 

i already update to the lasted S32DS. 

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

タグ(3)
0 件の賞賛
返信
9 返答(返信)

4,694件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please attach output from your debug console? 

Also make sure that the powerpc-eabivle-gdb.exe file is present in 

c:\NXP\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\bin\ 

folder and you can start it from windows command line:

pastedImage_1.png

Jiri

0 件の賞賛
返信

4,693件の閲覧回数
alex_yu1
Contributor III

hello,Jiri,

      check the  powerpc-eabivle-gdb.exe is under the right fold as following。

pastedImage_2.png

the debug console as following:

pastedImage_3.png

0 件の賞賛
返信

4,693件の閲覧回数
alexanderfedoto
NXP Employee
NXP Employee

Seems like you are trying to use wrong launch configuration.

Please make sure you have the following:

pastedImage_2.png

And correct prefix here

pastedImage_1.png

0 件の賞賛
返信

4,693件の閲覧回数
alex_yu1
Contributor III

hello 

      There are configuration for the debug interface

pastedImage_1.png

pastedImage_3.png

0 件の賞賛
返信

4,693件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is something wrong in project settings - but without project it is hard say where. Can you please share your project?

Jiri

0 件の賞賛
返信

4,693件の閲覧回数
alex_yu1
Contributor III

hello 

      it seems can not export the project setting,since it with processorexpert。

pastedImage_1.png

is it possible that the firewall will block the S32DS call the gbd.exe?  this project is the sample of S32DS.

pastedImage_2.png

thanks and regards

qingzhou 

0 件の賞賛
返信

4,693件の閲覧回数
alex_yu1
Contributor III

hello 

     i uninstall the symantec software , reinstall the S32DS, and there are another issue report when lauching.

pastedImage_1.png

0 件の賞賛
返信

4,693件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello alex_yu,

To share your project, please create a ZIP or similar archive of the project folder in your workspace. Then use the 'Use advanced editor' link in the comment window here to add the attachment.

pastedImage_1.png

Best Regards,

Mike

0 件の賞賛
返信

4,693件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is strange. Can you please share your project? 

Jiri

0 件の賞賛
返信