Error while running the program in S32 Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while running the program in S32 Design Studio

1,506件の閲覧回数
Krishna_Yalamanchili
Contributor I

Hi,

I am getting the following error when Run is pressed in S32 Design studio. I am trying to run after debug file is flashed and run. Please suggest what I have to do if i have to run the application only.

Error starting process.
Cannot run program "C:\Users\kyalamanchilli\workspaceS32DS.Power.2.1\hello_world_mpc5777c\Debug_FLASH\hello_world_mpc5777c.elf": Launching failed
Cannot run program "C:\Users\kyalamanchilli\workspaceS32DS.Power.2.1\hello_world_mpc5777c\Debug_FLASH\hello_world_mpc5777c.elf": Launching failed
Cannot run program "C:\Users\kyalamanchilli\workspaceS32DS.Power.2.1\hello_world_mpc5777c\Debug_FLASH\hello_world_mpc5777c.elf": Launching failed

0 件の賞賛
返信
1 返信

1,462件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Krishna_Yalamanchili,

Are you trying to just run or also debug?

If the application has been flashed successfully, then you just cycle the power to the board and it should run.

Best Regards,

Mike

0 件の賞賛
返信