Error when installing RTD 5.0.0 on S32DS 3.5.12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when installing RTD 5.0.0 on S32DS 3.5.12

693 Views
KMA
Contributor II

Hi S32 DS team,

 

I encountered this error while trying to install S32G RTD on top of S32DS 3.5 update 12 to use the DDR tool:   

KMA_0-1752160128435.png

Install works fine on S32DS 3.6.1, but I can't use the DDR tool due to python version issue (c.f DDR test validation don't work at S32 DS 3.6 - NXP Community)

 

Can you help, please

Thanks in advance

 

K.M.A

Tags (2)
0 Kudos
Reply
3 Replies

673 Views
carlos_o
NXP TechSupport
NXP TechSupport

Hi @KMA 

RTD 5.0.0 are tested under S32 Design Studio update 13

Could you please install the update 13 and try again to install the RTD 5.0.0?

0 Kudos
Reply

655 Views
KMA
Contributor II
Hi Carlos, thanks for the reply,
I tested on both updates 12 and 13 and I got the same error.
0 Kudos
Reply

645 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please make sure that you have S32DS updated to latest version (v3.5.14) and installed S32G2 development package prior to install RTD v5.0.0

jiri_kral_0-1752242164010.png

 

0 Kudos
Reply