Error loading programming algorithm on S32 debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error loading programming algorithm on S32 debugging

3,433 Views
jiahongdan
Contributor II

Hi,

 

Could you please help me to solve this problem?

The error loading programming algorithm ocurred when I started the debugging.

144443_144443.PNGerror[1].PNG

Hardware environment:  SCH-28455 REV B(daughter board) + KIT33908MBEVBE(mother boad).

 

Thank you in advance.

Labels (1)
Tags (1)
3 Replies

3,258 Views
stanish
NXP Employee
NXP Employee

Hello Dan,

Could you possibly check the board configuration jumpers?

I suspect SBC chip may reset the MCU prior flash programming algorithm is loaded.

Motherboard:

Please check if jumper JP112 is populated 1-2 : SBC Debug mode

Daughter card:

JP2 (VPP/TEST_MODE): 1-2

JP3 (RESET_PWSBC_B): OFF

JP7 (EXT_POR): OFF

Hope it helps!

Stan

3,258 Views
jiahongdan
Contributor II

Hello Stan,

I just find a always-succeed way to enter the debugging:

1.Press the RESET button of the daughter card

2.Click the debug icon of S32 design studio

3.Wait for the pop up window: "Reset Escalation"

4.Release the RESET button of the daughter card

5.Click the OK button of the S32 design studio's pop up window

Then, the debugging mode can be entered successfully.

Could you please tell me what I can do to simple the way of entering the debugging mode?

Jiahong DAN

0 Kudos
Reply

3,258 Views
jiahongdan
Contributor II

Hello Stan,

Thanks for your solution.

But it can not succeed every time. It failed mostly.

Could you please tell me how to improve this?

0 Kudos
Reply