Error in services launch sequence PEmicro GDB Launch Failure : Another GDB Server debug session is alreadyusing the same Server Port number. To run simultaneous debug sessions, please specify a unique Server Port and GDBMI Port in the Debug Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in services launch sequence PEmicro GDB Launch Failure : Another GDB Server debug session is alreadyusing the same Server Port number. To run simultaneous debug sessions, please specify a unique Server Port and GDBMI Port in the Debug Configuration

14,278件の閲覧回数
danieldu
Contributor II

Error in services launch sequence
PEmicro GDB Launch Failure : Another GDB Server debug session is alreadyusing the same Server Port number. To run simultaneous debug sessions, please specify a unique Server Port and GDBMI Port in the Debug Configuration for each project. If another session is not running simultaneously, make sure that the pegdbserver_console and the arm-none-eabi-gdb processes have terminated.

7 返答(返信)

11,057件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Make sure you don't have the debug session running (terminate it). Otherwise, see GDB Client and Server: Unlocking GDB | MCU on Eclipse 

I hope this helps,

Erich

11,057件の閲覧回数
tkdwofl
Contributor III

I don't understand...

i used S32K144 board when i work design studio.

PEGDBsever is not working..

Please help me!!

Can you explain me easily ?>

0 件の賞賛
返信

11,057件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The same thing applies to S32 Design Studio: have you checked your task list for another server running?

0 件の賞賛
返信

11,057件の閲覧回数
tkdwofl
Contributor III

pastedImage_1.png

stuck at Fault

when Ram Debug worked well. but Flash mode is happened Error.

  pastedImage_2.png

and  i can not find arm-none-eabi-gdb... 

0 件の賞賛
返信

11,057件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It would be pegdbserver_console.exe for P&E.

And check your launch configuration settings. It could be that your problem is this one: Solving “Launching: Configuring GDB Aborting Configuring GDB” | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信

11,057件の閲覧回数
tkdwofl
Contributor III

no..it is sill stuck on config..

how to reset Flash memory..?

0 件の賞賛
返信

11,057件の閲覧回数
tkdwofl
Contributor III

and How to execute Factory Reset on S32K144?

i push Reset button on board. but it is nothing.

i guess to reset RAM region.

i want to reset Flash region....

I do not speak well.. 

Thanks for taking my question. 

0 件の賞賛
返信