Error : Failed to execute MI command:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error : Failed to execute MI command:

6,283 Views
kihoon
Contributor I

Hello,

This is Kihoon Kim from Seoul National University of Science and Technology.

I have a question about S32 error.

How to solve this error??

Now I'm using S32 for Power Architecture, and MPC 5777 Development Board.

Error message is mentioned below.

Thank you.

Best Regards,

 

Error in final launch sequence
Failed to execute MI command:
-exec-run
Error message from debugger back end:
Error creating process C:/Users/kihoon/Dropbox/[3]°úÁ¦/[0]Çö´ëÀÚµ¿Â÷ Single stage 11kW OBC/[3]MPC5777C/Workspace/Hyundai_NXP_220713/SNU_CMU_mpc5777c/Debug_FLASH/SNU_CMU_mpc5777c.elf, (error 193).
Error creating process C:/Users/kihoon/Dropbox/[3]°úÁ¦/[0]Çö´ëÀÚµ¿Â÷ Single stage 11kW OBC/[3]MPC5777C/Workspace/Hyundai_NXP_220713/SNU_CMU_mpc5777c/Debug_FLASH/SNU_CMU_mpc5777c.elf, (error 193).

0 Kudos
Reply
6 Replies

6,073 Views
PaulSMagna
Contributor II

I am getting this same error . no space in the path 

Error in final launch sequence:

Failed to execute MI command:
-exec-run
Error message from debugger back end:
Error creating process C:\Work\NXP\flexcan_encrypted_s32k148\Debug_FLASH\flexcan_encrypted_s32k148.elf, (error 193).
Failed to execute MI command:
-exec-run
Error message from debugger back end:
Error creating process C:\Work\NXP\flexcan_encrypted_s32k148\Debug_FLASH\flexcan_encrypted_s32k148.elf, (error 193).
Error creating process C:\Work\NXP\flexcan_encrypted_s32k148\Debug_FLASH\flexcan_encrypted_s32k148.elf, (error 193).

I have checked the permissions on the folder and I have full access/write access for the folder system .. 

any thoughts. is there another folder it must write as well somewhere. that perhaps or which I do not have permissions. 

0 Kudos
Reply

6,067 Views
juan_see
Contributor III

Hi Paul, 

Where did you install your S32 Design Studio IDE? Could you please provide the full path?

 

0 Kudos
Reply

6,057 Views
PaulSMagna
Contributor II

Hi Juan

it is at 

C:\NXP\S32DS.3.4\eclipse

thanks for the assistance.

paul

0 Kudos
Reply

6,053 Views
juan_see
Contributor III

Hi Paul, 

Can you please try creating a blank application project for the S32K148? Does the issue also occurs there?

0 Kudos
Reply

5,469 Views
PaulSMagna
Contributor II
I have updated to ARM 2.2 and all is well
0 Kudos
Reply

6,125 Views
juan_see
Contributor III

Hi kihoon, 

Can you please visit the following link and try the suggestion? Please removing spaces in your path. 

https://stackoverflow.com/questions/1106930/cygwin-gdb-gives-error-193-when-trying-to-start-program

0 Kudos
Reply