EmbSysReg view bug in etpu address (MPC5746R)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EmbSysReg view bug in etpu address (MPC5746R)

1,433 次查看
merlinz
Contributor II

Hi. Yesterday after having many problems because my project was not going well I realized that the problem was that the addresses of the etpu in some are incorrect in EmbSysReg. I would like to know if there is any way to correct them since the records are not seen correctly.

By example, etpu_ccr_0 is 0xffcc0800 and correct is 0xffcc0400, also etpu_tb2r is tb1r and etpu_tb1r is tb2r.

There are many more errors in some address but I have not seen all of them.

Thanks.

2 回复数

1,325 次查看
jiri_kral
NXP Employee
NXP Employee

Hi David, 

this is known issue. Dev team is working on fix. Here is related thread:

https://community.nxp.com/thread/461701 

Jiri

1,325 次查看
merlinz
Contributor II

thanks, doing the search I did not see that thread.

0 项奖励
回复