EB activation failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB activation failed

Jump to solution
7,211 Views
yanzc
Contributor I

hello,I tried to activate the EB Tresos by using EB Client License Administrator V1.4.0 with the the following activation code:3147-F335-992C-A68A, it failed,here is the activation log:

INFO: Trusted Storage initialization done.
Activating NodeLocked License 3147-F335-992C-A68A, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.

 

How can I solve it , thank you!

0 Kudos
Reply
1 Solution
7,183 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @yanzc,

Probably the problem is from the connection from your local PC to the Elektrobit License Server. Try to activate online in another time, or you can try with offline activation, and the instruction can be found here: https://www.elektrobit.com/support/licensing/ (click to "Click here for offline instructions"). Otherwise, please contact to Elektrobit for better support.

Best Regards,

Nam

View solution in original post

0 Kudos
Reply
2 Replies
6,861 Views
heshuwen
Contributor I

Hi yanzc,

I having the same problem as you,Could you tell me how you solved it?

0 Kudos
Reply
7,184 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @yanzc,

Probably the problem is from the connection from your local PC to the Elektrobit License Server. Try to activate online in another time, or you can try with offline activation, and the instruction can be found here: https://www.elektrobit.com/support/licensing/ (click to "Click here for offline instructions"). Otherwise, please contact to Elektrobit for better support.

Best Regards,

Nam

0 Kudos
Reply