EB activation failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,404件の閲覧回数
yanzc
Contributor I

hello,I tried to activate the EB Tresos by using EB Client License Administrator V1.4.0 with the the following activation code:3147-F335-992C-A68A, it failed,here is the activation log:

INFO: Trusted Storage initialization done.
Activating NodeLocked License 3147-F335-992C-A68A, Number Of Licenses: 1
Status: 4, Creating request

Status: 5, Request created

Status: 6, Context created

Status: 0, Error

ERROR: flxActAppActivationSend (50041,41143,34)
Connection to FlexNet Operations Server failed.

 

How can I solve it , thank you!

0 件の賞賛
返信
1 解決策
7,376件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello @yanzc,

Probably the problem is from the connection from your local PC to the Elektrobit License Server. Try to activate online in another time, or you can try with offline activation, and the instruction can be found here: https://www.elektrobit.com/support/licensing/ (click to "Click here for offline instructions"). Otherwise, please contact to Elektrobit for better support.

Best Regards,

Nam

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
7,054件の閲覧回数
heshuwen
Contributor I

Hi yanzc,

I having the same problem as you,Could you tell me how you solved it?

0 件の賞賛
返信
7,376件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello @yanzc,

Probably the problem is from the connection from your local PC to the Elektrobit License Server. Try to activate online in another time, or you can try with offline activation, and the instruction can be found here: https://www.elektrobit.com/support/licensing/ (click to "Click here for offline instructions"). Otherwise, please contact to Elektrobit for better support.

Best Regards,

Nam

0 件の賞賛
返信