Does S32DS have a example project for MPC5644A PIT interrupt?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does S32DS have a example project for MPC5644A PIT interrupt?

Jump to solution
2,952 Views
alexhuang5367
Contributor I

Just like the title

Could any one provide a S32DS example for MPC5644A PIT interrupt.

I have this requirement because when i use CW2.1 my project is able to work, but turn to S32DS i can't open the interrupt 

when i open interrupt S32DS IDE just "Program received signal SIGTRAP, Trace/breakpoint trap.
0x00000004 in RCHW2 ()"

 

Please every one

Labels (1)
0 Kudos
Reply
1 Solution
2,767 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I described the problem to your previous thread.

MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? 

Here is the fixed project, which should work. Please try and let me know, if it works.

Regards,

Martin

View solution in original post

0 Kudos
Reply
1 Reply
2,768 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I described the problem to your previous thread.

MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? 

Here is the fixed project, which should work. Please try and let me know, if it works.

Regards,

Martin

0 Kudos
Reply