Does S32DS have a example project for MPC5644A PIT interrupt?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does S32DS have a example project for MPC5644A PIT interrupt?

ソリューションへジャンプ
2,888件の閲覧回数
alexhuang5367
Contributor II

Just like the title

Could any one provide a S32DS example for MPC5644A PIT interrupt.

I have this requirement because when i use CW2.1 my project is able to work, but turn to S32DS i can't open the interrupt 

when i open interrupt S32DS IDE just "Program received signal SIGTRAP, Trace/breakpoint trap.
0x00000004 in RCHW2 ()"

 

Please every one

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,703件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I described the problem to your previous thread.

MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? 

Here is the fixed project, which should work. Please try and let me know, if it works.

Regards,

Martin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,704件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

I described the problem to your previous thread.

MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? 

Here is the fixed project, which should work. Please try and let me know, if it works.

Regards,

Martin

0 件の賞賛
返信