Debugging using GDB Segger Jlink not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging using GDB Segger Jlink not working

2,243件の閲覧回数
shamika17
Contributor I

Using LPC LINK2 (jLINK) and Segger J-Flash Lite I was able to program FRDM-KEAZ128Q80 

 

Screenshot 2023-01-12 161902.pngScreenshot 2023-01-12 173653.png

But S32DS ARM2.2 IDE is giving me the Error in services launch sequence Starting J-Link GDB Server Timed out

 

I am using windows 11..please help as I want to debug

0 件の賞賛
返信
1 返信

2,207件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @shamika17,

How are you connecting the LPC-Link2 to the FRDM-KEAZ128Q80? Could you share a photo of the connection?

It is much easier to use the P&E OpenSDA connection for debug. Just connect USB cable to both your PC and the board.

Best Regards,

Mike

0 件の賞賛
返信