Debug Fail for empty device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Fail for empty device

2,203 次查看
leekate-b45752
NXP Employee
NXP Employee

Hello, 

When the user try to debug with empty device(S32K144) and S32DS v2.2, but it was failed to reset.

Could you guide about the issue? 

leekate-b45752_1-1607921669471.jpegleekate-b45752_1-1607921669471.jpeg

 

leekate-b45752_0-1607921634863.pngleekate-b45752_0-1607921634863.png

 

Best regards,

Kate Lee

0 项奖励
回复
2 回复数

2,196 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

 

um... interesting issue. Did you tried power cycle as suggested in output console? Also Emergency kinetis recovery may help. 

 

It is custom board or our EVB? 

 

BR, 

Jiri 

0 项奖励
回复

2,183 次查看
leekate-b45752
NXP Employee
NXP Employee

Hi Jiri, 

This issue was resolved by un-checked 'Use SWD protocol' box, but I couldn't understand the cause of the symptom. 

Best regards,

Kate Lee