Debug Fail for empty device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Fail for empty device

2,202件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hello, 

When the user try to debug with empty device(S32K144) and S32DS v2.2, but it was failed to reset.

Could you guide about the issue? 

leekate-b45752_1-1607921669471.jpegleekate-b45752_1-1607921669471.jpeg

 

leekate-b45752_0-1607921634863.pngleekate-b45752_0-1607921634863.png

 

Best regards,

Kate Lee

0 件の賞賛
返信
2 返答(返信)

2,195件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Kate, 

 

um... interesting issue. Did you tried power cycle as suggested in output console? Also Emergency kinetis recovery may help. 

 

It is custom board or our EVB? 

 

BR, 

Jiri 

0 件の賞賛
返信

2,182件の閲覧回数
leekate-b45752
NXP Employee
NXP Employee

Hi Jiri, 

This issue was resolved by un-checked 'Use SWD protocol' box, but I couldn't understand the cause of the symptom. 

Best regards,

Kate Lee