DIAB generate binary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,241件の閲覧回数
Ekaitz
Contributor II

Hello,

I'm usig the diab compiler and I can't generate the binary of my program. Someone knows how I can generate the binary?

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,207件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

I took the tool name from google, it looks that correct tool is  ddump.exe. The correct argument is probably ddump.exe -R my.elf my.srec - but I have no chance check or test it. 

 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,237件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you mean generate an .elf file or from existing .elf file generate .bin file? Is there some error message in build console? 

 

Jiri 

0 件の賞賛
返信
5,233件の閲覧回数
Ekaitz
Contributor II

Hello,

I want to generate .bin or .hex or .mot from the .elf.

At the begining is compile correctly.

Ekaitz_0-1614600429735.pngEkaitz_0-1614600429735.png

But it apeared two errors in the problems window.

Ekaitz_1-1614600489687.pngEkaitz_1-1614600489687.png

 

0 件の賞賛
返信
5,228件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately I don't have installed DIAB on my machine, but with DIAB toolchain it should be similar. Right click on project name -> Properties -> Settings and choose Cross Settings: 

jiri_kral_0-1614601165243.pngjiri_kral_0-1614601165243.png

 

Then press Apply button. You will see new section -Flash Image  in settings: 

jiri_kral_1-1614601281683.pngjiri_kral_1-1614601281683.png

 

If there is no such option - you may add a post build step with command:

mb-objcopy -O srec your_elf_file.elf your_srec_file.srec

 

jiri_kral_2-1614601412250.pngjiri_kral_2-1614601412250.png

 

Jiri 

 

 

 

 

 

0 件の賞賛
返信
5,227件の閲覧回数
Ekaitz
Contributor II

Thanks, but the configuration window is different from the GNU configuration window.

Ekaitz_0-1614601695187.pngEkaitz_0-1614601695187.png

I have also tried the command you say and it gives me an error.

Ekaitz_1-1614601740392.pngEkaitz_1-1614601740392.png

 

 

0 件の賞賛
返信
5,208件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

I took the tool name from google, it looks that correct tool is  ddump.exe. The correct argument is probably ddump.exe -R my.elf my.srec - but I have no chance check or test it. 

 

Jiri 

0 件の賞賛
返信