DIAB S32DS environment installed plugin SDK project after the project was founded after the processo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DIAB S32DS environment installed plugin SDK project after the project was founded after the processo

1,293 Views
lubo_NEW
Contributor III

In S32DS project, you want to set the input/output configuration of GPIO, etc., but the Pin Library Settings are not available As is shown inQQ图片20210303091646.png

0 Kudos
Reply
2 Replies

1,249 Views
mikedoidge
NXP Employee
NXP Employee

Hello @lubo_NEW ,

One way to make the view appear, select Hide Views from the Processor Expert menu, then Show Views. It should reopen the views for you. Otherwise you can manually add them from Window -> Show View -> Processor Expert.

image.png

mikedoidge_0-1615500049700.png

Hope it helps,

Mike

0 Kudos
Reply

1,291 Views
lubo_NEW
Contributor III

But the official instructions are shown in the figure for configuring pinsQQ图片20210303091537.png

0 Kudos
Reply