DIAB S32DS environment installed plugin SDK project after the project was founded after the processo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DIAB S32DS environment installed plugin SDK project after the project was founded after the processo

1,291 次查看
lubo_NEW
Contributor III

In S32DS project, you want to set the input/output configuration of GPIO, etc., but the Pin Library Settings are not available As is shown inQQ图片20210303091646.png

0 项奖励
回复
2 回复数

1,247 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @lubo_NEW ,

One way to make the view appear, select Hide Views from the Processor Expert menu, then Show Views. It should reopen the views for you. Otherwise you can manually add them from Window -> Show View -> Processor Expert.

image.png

mikedoidge_0-1615500049700.png

Hope it helps,

Mike

0 项奖励
回复

1,289 次查看
lubo_NEW
Contributor III

But the official instructions are shown in the figure for configuring pinsQQ图片20210303091537.png

0 项奖励
回复