DDR test validation don't work at S32 DS 3.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR test validation don't work at S32 DS 3.6

1,108 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Hi S32 DS team,

Using S32 Design Studio version 3.6.0, build ID 241128, on Windows 11. When running any (f.e. Firmware Init Test) for the DDR, get following error. Apparently S32G SDK scripts use python version 2, whereas the installation of S32 Design studio has python3(S32DS\build_tools\msys32\mingw64\bin) and python2(S32DS\build_tools\msys32\mingw32\bin).

Tianxiang_Huang_0-1737698680587.png

Seems the tool use python3 but the script is python2. 

How could you fix this bug, can S32DS DDR tool config which python version to use. Or update the DDR tool python script thanks!

BRs,

Tianxiang

Labels (1)
0 Kudos
Reply
4 Replies

460 Views
KMA
Contributor II

Hello S32DS team,

 

I am facing the same problem with S32DS 3.6.1, is there any solution to this issue? 

0 Kudos
Reply

453 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Hi Mohamed, 

 

What RTD version is the customer using? Please check if the RTD version matches the S32DS.

Following is the analysis in the Jira ticket.

Tianxiang_Huang_1-1751592027760.png

 

BRs,

Tianxiang

0 Kudos
Reply

1,018 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please create JIRA ticket on our internal pages for this bug. It looks, that the python script is not properly ported from Python 2.7 to Python 3. 

0 Kudos
Reply

983 Views
Tianxiang_Huang
NXP Employee
NXP Employee

Got it, Thanks!

BRs,

Tianxiang

0 Kudos
Reply