DDR test validation don't work at S32 DS 3.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR test validation don't work at S32 DS 3.6

1,018件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Hi S32 DS team,

Using S32 Design Studio version 3.6.0, build ID 241128, on Windows 11. When running any (f.e. Firmware Init Test) for the DDR, get following error. Apparently S32G SDK scripts use python version 2, whereas the installation of S32 Design studio has python3(S32DS\build_tools\msys32\mingw64\bin) and python2(S32DS\build_tools\msys32\mingw32\bin).

Tianxiang_Huang_0-1737698680587.png

Seems the tool use python3 but the script is python2. 

How could you fix this bug, can S32DS DDR tool config which python version to use. Or update the DDR tool python script thanks!

BRs,

Tianxiang

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

370件の閲覧回数
KMA
Contributor II

Hello S32DS team,

 

I am facing the same problem with S32DS 3.6.1, is there any solution to this issue? 

0 件の賞賛
返信

363件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Hi Mohamed, 

 

What RTD version is the customer using? Please check if the RTD version matches the S32DS.

Following is the analysis in the Jira ticket.

Tianxiang_Huang_1-1751592027760.png

 

BRs,

Tianxiang

0 件の賞賛
返信

928件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please create JIRA ticket on our internal pages for this bug. It looks, that the python script is not properly ported from Python 2.7 to Python 3. 

0 件の賞賛
返信

893件の閲覧回数
Tianxiang_Huang
NXP Employee
NXP Employee

Got it, Thanks!

BRs,

Tianxiang

0 件の賞賛
返信