Create An ISP Project From Existing VSDK Graph in S32DS3.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create An ISP Project From Existing VSDK Graph in S32DS3.1

1,026件の閲覧回数
751301185
Contributor II

Hi,

When I create an ISP Project From Existing VSDK Graph using S32DS3.1,code emit has been completed.

Expand the folders within Camera_test_Demo, A53_gen, src and inc, no the newly generated output files.

/home/lilei/NXP/S32DS.3.1/S32DS/tools/clt/isp/1.0.0/bin/runItByIDE.sh: 行 24: java: 未找到命令

Can anyone help me solve this problem? Thank you

pastedImage_1.pngpastedImage_2.png

/home/lilei/NXP/S32DS.3.1/S32DS/tools/clt/isp/1.0.0/bin/runItByIDE.sh   The contents of the script file are as follows:

pastedImage_3.png

pastedImage_4.png

タグ(3)
0 件の賞賛
返信
0 返答(返信)