Create A New Makefile Project With Existing Code failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create A New Makefile Project With Existing Code failure

3,120 Views
635986562
Contributor I

Hi,I have installed S32DS.Vision.2018.R1,but I got a problem.I created a new makefile project according to the documentation:HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project 

After I created the project ,I can't find the graph file and there was only one build configuration:default.How can I creat a project like that in the documentation?

微信图片_20190802163605.jpg

0 Kudos
Reply
2 Replies

2,892 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I updated the HowTo document related to Makefile project. Make sure that on Linux host you added paths in Unix style. 

https://community.nxp.com/docs/DOC-335012 

Hope it helps. 

Jiri 

0 Kudos
Reply

2,892 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that there are missing some steps in this howto. Also some images are misleading. I'll update this Howto and let you know. 

Anyway, what is your use case to import Makefile project? Almost all demos for from VSDK are available as normal S32DS Example - File -> New -> S32DS Project from Example. You don't need import it as Makefile project. 

 

pastedImage_1.png

Jiri 

0 Kudos
Reply