Change processor inside S32DS V3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change processor inside S32DS V3.4

Jump to solution
2,590 Views
superbird
Contributor I

Hello, 

is there a way to change the processor type inside a S32DS project?

I need to change from S32K144 to S32K146 but can only find the dialog to select different package of the same processor.

superbird_0-1671174655409.png

Thanks for any help.

Best Regards,

0 Kudos
Reply
1 Solution
2,576 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @superbird 

I am afraid that the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience

 

B.R

VaneB

View solution in original post

0 Kudos
Reply
1 Reply
2,577 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @superbird 

I am afraid that the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience

 

B.R

VaneB

0 Kudos
Reply