Change processor inside S32DS V3.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change processor inside S32DS V3.4

ソリューションへジャンプ
2,580件の閲覧回数
superbird
Contributor I

Hello, 

is there a way to change the processor type inside a S32DS project?

I need to change from S32K144 to S32K146 but can only find the dialog to select different package of the same processor.

superbird_0-1671174655409.pngsuperbird_0-1671174655409.png

Thanks for any help.

Best Regards,

0 件の賞賛
返信
1 解決策
2,566件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @superbird 

I am afraid that the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience

 

B.R

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,567件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @superbird 

I am afraid that the most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience

 

B.R

VaneB

0 件の賞賛
返信