Can't program S32K148EVB-176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't program S32K148EVB-176

1,343 Views
smile9999
Contributor I

I have got a S32K148EVB-176 board and run some examples. The debug_flash setting won't work while debug_RAM works fine.

I have refered to below link, not working.

https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/963204

Any advice is appreciated. Thanks.

0 Kudos
Reply
2 Replies

1,342 Views
smile9999
Contributor I
Console log attached: ;version 1.05, 12/03/2019, Copyright 2019 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [s32k148f2m0m11_x_pflash_dflash_eeprom] ;device freescale, s32k148f2m0m11, pflash_dflash_eeprom ;begin_cs device=$00000000, length=$14001000, ram=$20000000 Loading programming algorithm ... Done. Programming sequency is : erase, blank check, program, and verify {default} CMD>VC Verifying object file CRC-16 to device ranges ... block 00000000-0000340F ... Error! CRC Command Timed Out Current content of flash does not match application to be programmed CMD>EM Command is inactive for this .ARP file. Error Erasing flash of device Error occured during Flash programming. PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.
0 Kudos
Reply

1,341 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please check in Debug configurations -> advanced options if you are using default flash algorithm: 

jiri_kral_0-1599054001042.png

jiri_kral_1-1599054056750.png

 

Jiri

 

 

0 Kudos
Reply