Can't install TCPIP 1.0.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't install TCPIP 1.0.3

4,962 次查看
cw20
Contributor II

Hi,

I cannot install TCPIP v1.0.3 onto DS 3.5. I installed all the required packages and the correct versions. I've tried adding it through the extension and updates window as well as the "install new software" option but both do not work. As a result, the lwip example is not available. What should I do?

 

I've included all the packages I have installed in a txt file.  

标记 (3)
0 项奖励
回复
5 回复数

4,906 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cw20 ,

Please ca you share the Workspace installation log to understand the issue. 

From Path

C:\Users\Public\[Woskapce_name]\.metadata 

(or wherever your workspace is located. 

Thank you. Best regards. 

- Mehul Patel

 

0 项奖励
回复

4,410 次查看
shunyizhang
Contributor IV

Hi @Mehul_Patel_NXP ,

any updates on how to fix this issue?

0 项奖励
回复

4,886 次查看
cw20
Contributor II

Hi @Mehul_Patel_NXP 

Here's the workspace installation log. Thanks

0 项奖励
回复

4,844 次查看
cw20
Contributor II

Hi @Mehul_Patel_NXP ,

any updates on how to fix this issue?

0 项奖励
回复

4,831 次查看
bwp530
Contributor IV

same issue

0 项奖励
回复